Motor_SYNC
Motor_SYNC
| Address: | 8832 (2280H) |
| Type: | WORD |
| Access: | Write Only |
| Unit: | -- |
| Range: | 0 to 1 |
| Default Value: | 0 |
| Store Supported: | No |
| Description: | This object is used to synchronize the start and the stop of movement that must be synchronized between more axes. |
| Notes: | See Movements with SYNC for details about synchronized movements. |